Technical FAQs

Ask a Question

List troubleshooting points for PowerLogic PM5350 on potential problems (symptons) and possible solutions.

Symptoms Possible causes
Negative kW Reverse power flowing
CT connections reversed
Negative pf and VAR Pf is capacitive
Device not communicating Check device id/baud rate/Parity
Check RS485 connections/cable / converter
kWh  negative Reverse power flowing
CT connections reversed
kW & kWh total readings incorrect Reverse power flowing
CT connections reversed
Integrator starting from “0” Check the Old Intg values stored for reference
If required change the overflow settings
Was this helpful?
What can we do to improve the information ?