Technical FAQs

Ask a Question

What is the risk of damage to the user and PowerLogic energy meters.

Statuatory Notice:
  • Wear suitable protection equipments and follow the applicable Electrical Safety Instructions to avoid serious injury.
  • Never OPEN the Energy meter unit
  • Do not attempt to repair any components in the Energy meter range, either in the unit or the accessory.
  • Failure to follow these Instructions can result in equipment damage.
Was this helpful?
What can we do to improve the information ?