Technical FAQs

Ask a Question

What is the maximum numbers of TCP connections ZBRN1 access point supports

ZBRCETH is a communication module that supports Ethernet Modbus/TCP protocol. It is to be inserted in ZBRN1 access point.
Maximum numbers of TCP connections supported by ZBRN1 access point is 6.
If more than 6 connections are requested, the connection with oldest transaction will be closed to allow new connection.
Was this helpful?
What can we do to improve the information ?