Technical FAQs

Ask a Question

How can I setup the LAN port redundancy with my Vijeo Citect 7.40 software project as on my PC I have dual lan ports available.

You need to create two network address like Net1 and Net2 and then use these two network names in your all the Servers with (,) comma as shown in the attached snapshot.
Was this helpful?
What can we do to improve the information ?