Technical FAQs

Ask a Question

What is the material and the component used for heat sink in our ABL1REM24062 power supply.

There are 3 heat sinks for ABL1REM24062 and the material information are as below for your reference. 

HS1(COPPER) : CU1100 
HS2(ALUMINUM) : AL1100 
HS3(ALUMINUM) : AL1100 
Was this helpful?
What can we do to improve the information ?