Technical FAQs

Ask a Question

Can i use a cable fast cabling to wire up Modicon Quantum 140 ATI 030 00 thermocouple module.

For wiring up 140ATI 030 00 module, the 140 CFA 040 00 CableFast block can be used. However it can create a temperature variation up to 35.6 °F (2 °C). The reason for this variation is, 140CFA04000 block does not incorporate an isometric barrier. Without such a  barrier, temperature readings may vary up to 2 degrees from one end of the block to the other. If the application can tolerate this temperature error, the block (and module remote CJC) may be used.
Was this helpful?
What can we do to improve the information ?