Technical FAQs

Ask a Question

How is the connection schematic of the IFE to a Fixed or Drawout Masterpact NT/NW or PowerPact P- or R-Frame circuit breaker for system voltage greater than 480 Vac.

Please refer below the connection schematic of the IFE to a Fixed or Drawout Masterpact NT/NW or PowerPact P- or R-Frame circuit breaker for system voltage greater than 480 Vac.

Was this helpful?
What can we do to improve the information ?