Technical FAQs

Ask a Question

For the setting of the PTC probe in the fault management, if we set it to Motor On, will the sensing of the LI6 happen when the Altivar 71 drive sends run command to motor.

If you set PtCL to [Motor ON], then it will monitor the resistance Value when the VSD sends a run command to motor.

For information:
Input for a PTC probes mounted in series:
- Nominal value < 1.5 kOhm
- Trip resistance 3 kOhm, reset value 1.8 kOhm
- Short-circuit protection < 50 Ohm
Was this helpful?
What can we do to improve the information ?