Technical FAQs

Ask a Question

In UPS BX1000UXI power on/off button is flashing for every 2sec with beep sound?

  • It indicates UPS is in Overload indication or may be short circuit at the output.
  • Check with customer how much watt load connected to the UPS (not exceeding 600W for BX1000UXI/1200W for BX2000UXI).
  • Disconnect non-essential equipment one device at a time to reduce the overload condition.
  • Restart the UPS until the overload indication or issue has been resolved.
Was this helpful?
What can we do to improve the information ?