Technical FAQs

Ask a Question

UPS tripped due to Overload in UPS BX1000UXI?

  • Disconnect the entire load connected to UPS.
  • Reset the Circuit Breaker present at the back panel of UPS.
  • Reconnect the equipment one at a time, if circuit breaker trips again disconnect the device that caused problem.
  • Power on the UPS through Power ON/OFF button.
Was this helpful?
What can we do to improve the information ?