Technical FAQs

Ask a Question

UPS is giving beep sound and power on/off light flashing for every 6 seconds in UPS BX1000UXI?

  • Check the temperature of the site.
  • See that UPS is kept under better ventilation.
  • Check the UPS if it is overheated by touching it.
  • Disconnect non essential equipment connected to UPS to correct this error.
  • UPS will beep red light indication still the internal temperature reaches normal.
Was this helpful?
What can we do to improve the information ?