Technical FAQs

Ask a Question

Charging LED is flashing for every 5 sec with beep sound in UPS BX1000UXI?

  • It indicates that battery is not connected properly with the UPS.
  • Check the battery connection of the UPS.
  • Shutdown the UPS and check whether cables are correctly connected to the terminals of the battery. i.e. polarity of the Battery.
  • Restart the UPS and check any beep sound, if still problem persist contact customer care. 
Was this helpful?
What can we do to improve the information ?