Technical FAQs

Ask a Question

Is there a way to download/upload application to LMC078 motion controller with removable memory device such as USB memory stick or SD card like LMC058 or M241.

There is no possibility as of now to download the application via removable memory device such as USB or SD card. The only possibility is to download the application using USB cable or Ethernet. 

However there is a possibility to clone the application from one controller to another by reading the image from one controller and write the image to SD card or USB drive using Controller Assistant. 
Was this helpful?
What can we do to improve the information ?