Technical FAQs

Ask a Question

How can we use Citect Project DBF add-in in Excel 64 bit version machine.

An Excel 64-bit compatible version of the Project DBF Add-in is not available at this stage. It is recommended that you install the 32-bit version of Excel should you wish to use the Project DBF Add-in. 
Was this helpful?
What can we do to improve the information ?