Technical FAQs

Ask a Question

Does LXM32M servo drive support ProfiNet option card of ATV32.

The Profinet Option card of ATV32 do not work in LXM32. Presently there is not any option module available for Profinet in LXM32.

The workaround for you is to use Profibus Option Module in LXM32 and use PROFIBUS to PROFINET PROXY from HILSCHER or any third party Gateway solution.
Was this helpful?
What can we do to improve the information ?