Technical FAQs

Ask a Question

Is RM35TF30 multifunction 3-phase supply control relay suitable to operate with supply networks having harmonic distortions

RM35TF30 multifunction 3-phase supply control relay is using true RMS measurement method to analyze the input signals.
It can function correctly even if the voltage harmonic distortion signals present in the network system. 
This product has been validated with different kind of voltage harmonic distortion signals with maximum level of THD up to 45.84%

(THD = Total Harmonics Distortion)
Was this helpful?
What can we do to improve the information ?