Technical FAQs

Ask a Question

Can analog inputs of zelio smart relay be used as discrete inputs

Yes, analog inputs can be usable as discrete inputs depending on zelio smart relay model.
To have this, analog input needs to be configured as discrete input in zeliosoft2 programming software.
Refer to the below snap.
When cursor is pointed to IE analog input, it shows DISCR / ANA indicating can be configurable as either discrete input or analog input.



For example, zelio smart relay SR3B201BD with its 4 analog inputs. Refer to below snap to show the configuration of one of analog input as discrete input.
Step-1
Selection of discrete input.



Step-2
In this example, Analog input IE is configured as discrete input. Refer to below snap.


 
Was this helpful?
What can we do to improve the information ?