Technical FAQs

Ask a Question

What are the functions performed by BSCM (Breaker Status and Control Module) used in Compact NSX.

The BSCM (Breaker Status and Control Module) performs the:
  • Status indication functions for the Compact NSX circuit breaker
  • Control of the communicating motor mechanism
  • Operating assistance functions
The BSCM can be used with thermal-magnetic and Micrologic electronic trip units.
Was this helpful?
What can we do to improve the information ?