Technical FAQs

Ask a Question

What is the function of Isolated NSX Cord used in Compact NSX.

For applications > 480 VAC, an isolated variant of the NSX cord needs to be used, terminated by an electronic module with a female RJ45 connector. A ULP¨cord must be used to connect the isolated NSX cord electronic module to a ULP module.
The reference for the isolated NSX Cord is LV434204.
The isolated NSX cord electronic module must be supplied with 24 VDC in order to guarantee isolation of the ULP system.
Was this helpful?
What can we do to improve the information ?