Technical FAQs

Ask a Question

Describe the connections with Ethernet Gateway and 24VDC power supply with Modbus communication interface module (TRV00210).

The wiring diagram below shows the connections for the EGX or MPS100 Ethernet gateway and the 24 VDC power supply in detail;
Was this helpful?
What can we do to improve the information ?