Technical FAQs

Ask a Question

Which devices can be monitored through FDM128 when an Acti 9 Smartlink is connected to it.

When an Acti 9 Smartlink is connected to the FDM128, the status of the devices connected through the Acti 9 Smartlink can be viewed on the FDM128.
The status of the following devices can be viewed on the FDM128 are:
> Acti 9 iOF+SD24 and OF+SD24 indication auxiliaries
> Acti 9 iACT24 and iATL24 auxiliaries for contactors and impulse relays in the Acti 9 range
> Acti 9 RCA iC60 remote control module with Ti24 interface
> Acti 9 Reflex iC60 integrated control circuit breaker with Ti24 interface
> iEM2000T, iEM3110, iEM3155, iEM3210 and and iEM3255 energy meters
> Compact NSX OF+SD indication auxiliaries
Was this helpful?
What can we do to improve the information ?