Technical FAQs

Ask a Question

What are the standards to which Enerlin'X FDM128 comply to.

The FDM128 display unit complies with the following standards:
> IEC 60947-1 general rules
> UL 508, Industrial Control Equipment
> CSA C22.2 No. 14-05 Industrial Control Equipment
> IACS E10

 
Was this helpful?
What can we do to improve the information ?