Technical FAQs

Ask a Question

How to reset XBKH70000002M counter

XBKH70000002M is an electromechanical one and has no reset means.
Its functioning principle is an electromagnetic which actuate a cam and this one turn a wheel, this is not reversible.
The reset function for this product was not foreseen by the designer.
In case of XBKH70000002M counter reaches full range value (e.g., 99 999.99 h) then  afterwards it will begin 0 again.
Was this helpful?
What can we do to improve the information ?