Technical FAQs

Ask a Question

What are the directives and standards to which FDM128 complies for the Hazardous substances.

The FDM128 display unit is designed for compliance with the following directives and standards:
> WEEE, Directive 2002/96/EC
> RoHS, Directive 2002/95/EC
> RoHS China, Standard SJ/T 11363-2006
Was this helpful?
What can we do to improve the information ?