Technical FAQs

Ask a Question

What is the DIP switch settings for two IO Module Addressing.

When 2 IO modules are connected in the same ULP network used in one IMU, the 2 IO modules are
.differentiated by the position of the DIP switch located on the bottom of the IO module . Please refer attachment.
Was this helpful?
What can we do to improve the information ?