Technical FAQs

Ask a Question

How to migrate from Unity pro v2.3 to Unity pro v10

If you does not have a valid subcription package then you should order Expired Subscription Services
 
UNYCSPSPUEEU EXP SUB PRO XL SINGLE LICENCE

By ordering this you would get :- 
  • DVD Unity Pro V10 in 6 Languages (EN, FR, SP, GE, IT, CN)
  • CD Advantys Configuration Software V8.0
  • One-year subscription service
  • License(s) depending the Unity Pro model
 Note : A new licence is delivered with expired subscription packages. But it is mandatory to have a valid Part Number / Serial Number to be able to get a new authorization code i.e details of the old license v2.3.

After receiving this package you should install UNYCSPSPUEEU on new computer . When Serial Number / Part Number is required during installation, prompt PN UNYCSPSPUEEU / SN  ZZZZZZZ). Contact SE customer care center, to get a new authorization code : you have to provides UNYCSPSPUEEU / ZZZZZZZ PN / SN information,  and the old UNYSPUEFUCD23 /  XXXXX in addition to check the link with expired subscription service i.e of v2.3. 
Was this helpful?
What can we do to improve the information ?