Technical FAQs

Ask a Question

Does the BMXPRA0100 also contains same type of Rotatory Switches as M340 cpu for configuration of IP address.

The Modicon M340 module BMXPRA0100 and CPUs with Ethernet functionality can have their addresses set through the rotary switches, or the Unity Pro IP Configuration tab, and combinations of the two. Refer to the enclosed for complete information.
Was this helpful?
What can we do to improve the information ?