Technical FAQs

Ask a Question

Do Vijeo Citect have the feature of Alarm output as text to speech.

There is no such default feature available in Vijeo Citect SCADA for Pronunciation of Voice Alarms. You can only do it by recording the wav file and play it as respective alarm triggers. 

However if you are familiar with some customized programming code such as .Net or VB then you can use it to connect to Vijeo Citect Alarm Database and generate such text to speech alarm output.
Was this helpful?
What can we do to improve the information ?