Technical FAQs

Ask a Question

Can we use extracted bit of Array Variable in Vijeo Designer.

The bit extraction from Array Variable is not supported in Vijeo Designer you will have to create new variable in Vijeo Designer for each located address in PLC. 

For variable other than Array or Structure, you can use Variable Methods to read extracted bit and write to extracted bit of an Integer variable. 
Was this helpful?
What can we do to improve the information ?