Technical FAQs

Ask a Question

How to set the threshold in Back-UPS BR1000G-IN / BR1500G-IN ?

1. Ensure a master device is connected to the Master outlet. Put that device
into Sleep or Standby mode, or turn it OFF.
2. Press DISPLAY and MUTE simultaneously and hold for six seconds, until
the leaf icon flashes three times and the Back-UPS beeps three times.
3. The Back-UPS will now recognize the threshold level of the Master
device and save it as the new threshold setting.

Setting the threshold. The amount of power used by a device in Sleep or
Standby mode varies between devices. It may be necessary to adjust the
threshold at which the Master outlet signals the Controlled outlets to shut
Was this helpful?
What can we do to improve the information ?