Technical FAQs

Ask a Question

How to Disable the power-saving function in Back-UPS BR1000G-IN / BR1500G-IN ?

Press and hold MUTE and DISPLAY
simultaneously for two seconds. The Back-UPS will beep to indicate that the
feature is disabled. The leaf icon on the display will clear out.
Was this helpful?
What can we do to improve the information ?