Technical FAQs

Ask a Question

What to do if Back-UPS BR1000G-IN / BR1500G-IN is not showing anything on display ?

This is due to Display Power-Saving mode .

To turn on the display , follow below steps.

Press and hold DISPLAY button for two seconds. 

NOTE :While in Power-Saving Mode, the display will illuminate
if a button is pressed, it then goes dark after 60 seconds of no activity.
Was this helpful?
What can we do to improve the information ?