Technical FAQs

Ask a Question

What is the maximum inrush current for the safety relay XPS AC 5121 with some supporting documents.

This attached resolution page as shared for your reference which clarifies that for the XPS AC 5121 relay the maximum Inrush current value is 3 Amps (< 3 ms) and at nominal voltage it is less than 2.5 Amps . 
Was this helpful?
What can we do to improve the information ?