Technical FAQs

Ask a Question

With VJC 7.40 in process analyst view when we put cursor in trend label shows correct date-time but in object area cursor date-time shows wrong, how can we resolve this problem.

In Process Analyst , the cursor time label was correct but the cursor time column was wrong by the local time zone offset. For example, if the local time zone offset was +10 hours, the column value would be 10 hours ahead of the cursor time label. This has been fixed in the attached hotfix HF740SP162508 . 

Kindly download this hotfix HF740SP162508 from the below link : 

You need to install this hotfix over Vijeo Citect 7.40 Sp1 . 
Was this helpful?
What can we do to improve the information ?