Technical FAQs

Ask a Question

In Vijeo Citect runtime minimize option should be configurable for a particular user group so that it will allow to minimize runtime screen only if that particular user/persons logs in.

There is no built in way to make the minimize button in the top right of runtime windows only available for specific users for minimize window. 

But what you can do is create a new button that uses this function of Vijeo Citect WinMode(7) and you can set whatever visibility or privilege you want on that button so that it is available for any user you want. 
Was this helpful?
What can we do to improve the information ?