Technical FAQs

Ask a Question

Which Virtual machine is supported by Vijeo Citect and what considerations we need to follow to use the Vijeo Citect licensing with virtual machine.

There are an increasing number of customers now using virtual machines to host SCADA runtime servers. The only virtual machine environment tested and supported is VMWare Workstation and VMWare ESX. Kindly check the attached document for more details on licensing of Vijeo Citect with Virtual machines.
Was this helpful?
What can we do to improve the information ?