Technical FAQs

Ask a Question

Does the protection on ATS48 Soft Starter work when it is switched to bypass mode.

There is no special protection functions package active when by-pass operated. The soft starter has no information whether it bypassed or not, there is no feedback from the bypass contactor, current flows through CT =>So, all the protections stay active when it is switched to bypass mode.
Was this helpful?
What can we do to improve the information ?