Technical FAQs

Ask a Question

Is it possible to use Multi-Loader with ATV303 drive.

Yes, it is possible.ATV303 configuration file can be copied to the Multi-Loader and then transfers the configuration file from the Multi-Loader to the ATV303 drives.
Was this helpful?
What can we do to improve the information ?