Technical FAQs

Ask a Question

How to configure 140CPU67261 to operate in RUN Primary mode without usage of 140CRP module.

For a Quantum HSBY plc (140CPU67xxx) to be in RUN Primary mode, CRP is must, however CRA is not mandatory. To use the HSBY cpu as standalone without any drop, you can connect the two Device Network ports on the CRP module with each other (dummy connection).

 
Was this helpful?
What can we do to improve the information ?