Technical FAQs

Ask a Question

What is the device name (over DHCP) for IP address assignment of BMXPRA0100 module.

BMXPRA0100 IP address could be assigned by using the rotary switches on the back of module. You should use name as BMX_0100_xxy where xxy is the value derived from the dip switch position. xx is the value of the upper rotary switch and y is the value of the lower rotary switch.
Was this helpful?
What can we do to improve the information ?