Technical FAQs

Ask a Question

What to do if I forgot the password of the application (project) in Unity Pro XL Software

If you forget your password, contact the Schneider Support. There are two cases: 
1. You forgot the password of the application (project) in Unity Pro XLS Software needed to open a project or at the auto-lock situation.
2. You forgot the password of the application that is in the PLC.

Please refer to the enclosed doc for more info.
Was this helpful?
What can we do to improve the information ?