Technical FAQs

Ask a Question

Is all the system bit and words are supported for Quantum Safety controllers.

Not all of the system bits and words can be used in the Quantum Safety PLC. The unusable system bits are marked in the Quantum Safety column with no.
Refer the enclosed document to find the supported system bit and word with Quantum Safety PLCs.
Was this helpful?
What can we do to improve the information ?