Technical FAQs

Ask a Question

What is the maximum length between M580 PLC and last extension drop.

The maximum distance between M580 plc and last extension drop should be less than 30meters .The maximum Extension cable length is 12m. Refer the below mentioned part references of cable.

BMXXBC008K = Backplane extension cable 0.8M 

BMXXBC015K = Backplane extension cable 1.5M 

BMXXBC030K = Backplane extension cable 3M 

BMXXBC050K = Backplane extension cable 5M 

BMXXBC120K = Backplane extension cable 12M
Was this helpful?
What can we do to improve the information ?