Technical FAQs

Ask a Question

Does the Modicon Quantum PLC have the capability to issue an alarm if the CPU gets over heated

The operating conditions in terms of temperature for Modicon Quantum plc is 0 ... 60 °C (32 ... 140 °F), however this parameter is not monitored internally by the module or any system word.
Was this helpful?
What can we do to improve the information ?