Technical FAQs

Ask a Question

What is the difference between 170FNT11000 and 170FNT11001, Can we use these adaptors with 170ADI35000(IO Base).

170FNT11000 and 170FNT11001 both are Fipio communication adaptor and both can be used with 170ADI35000(IO Base).
The basic different between these two are as follows:

Bus manager PLC:

For 170FNT11000 = TSX series 7, model 40 or April 5000
For 170FNT11001 = Premium

Number of devices:

For 170FNT11000:=
0...61 all segment with repeater
0...31 per segment without repeater

For 170FNT11001:=
0...97 all segment with repeater
0...31 per segment without repeater

Datasheets for both are enclosed.
Was this helpful?
What can we do to improve the information ?