Technical FAQs

Ask a Question

What are the Modicon Quantum module restriction in Unity Pro.

: The Quantum Hot Standby with Unity Pro V2.0 and later versions do not support the following modules.
  • 140 NOE 311 00
  • 140 NOE 351 00
  • 140 CHS 110 00
  • 140 NOA 611 10
  • 140 NOA 622 00
  • 140 NOL 911 10
  • 140 HLI 340 00 
Was this helpful?
What can we do to improve the information ?