Technical FAQs

Ask a Question

What are the network addresses for different protocols during switchover in Quantum Hot standby system.

Quantum Hot Standby system can communicate data over different network protocols:
  • Modbus
  • Modbus Plus
  • TCP/IP
In Hot Standby applications, correct address assignment must be fulfilled for proper operation of network address swap at switchover.
Refer the attached document to understand the network address during switchover for different protocols.
Was this helpful?
What can we do to improve the information ?