Technical FAQs

Ask a Question

How to check the Firmware Mismatch of the components installed in Local rack of Quantum Hot Standby system.

Bits in the Firmware Mismatch Register (%SW69)
The Hot Standby Firmware Mismatch Register, %SW69, gives information about the firmware levels in the Primary and Standby main rack components:
  • The firmware levels in the Primary and Standby CPUs, Copros and Ethernet CRPs are compared:
  • If a bit = 0, the Primary and Standby components have the same firmware versions.
  • If a bit = 1, the Primary and Standby components have different firmware versions.
  • Bits 0 to 15 correspond to rack positions 16 to 1:
Refer the attach file.
 
Was this helpful?
What can we do to improve the information ?