Technical FAQs

Ask a Question

What is the output contact rating of Acti9 low level interface iRBN relay.

The output contact rating of Acti9 low level interface iRBN relay is :

Minimum >  5 mA/5 V DC (DC12)
                  5 mA/5 V AC

Maximum > 1 A/24 V DC (DC12)
                   5 A/250 V AC
Was this helpful?
What can we do to improve the information ?