Technical FAQs

Ask a Question

What is the output contact rating of Acti9 extra low voltage iRTBT interface relay.

The he output contact rating of Acti9 extra low voltage iRTBT interface relay is:

-> Minimum >  10 mA/10 V DC (DC12)
                      10 mA/10 V AC
-> Maximum > 1 A/24 V DC (DC12)
                      5 A/250 V AC
Was this helpful?
What can we do to improve the information ?